GP BJT
A general purpose bipolar junction transistor (GP BJT) is a very versatile device that can be used as a current or voltage-controlled switch and also as an amplifier. It can be used to design a host of different types of circuits such as filters, receivers, transmitters, operational amplifiers, power supplies, and control circuits to name a few. A BJT is a three terminal device (base, emitter and collector) and is available in one of two complementary forms (NPN and PNP). When the terminal voltages are biased in the correct polarity, a current flows between the collector and emitter that are proportional to the current that is present between the base and emitter terminal. The ratio of the collector to the base current is called the gain or beta of the transistor. The behavior of NPN and PNP types are almost identical, except that the bias voltages and controlling currents have opposite polarities. When selecting a BJT, many characteristics should be considered including absolute maximum ratings, thermal characteristics, and DC and AC electrical characteristics.
10,608
์ด ์ ํ