광전자공학
Arrow.com is an authorized distributor of optoelectronics from leading manufacturers including onsemi, Everlight, Vishay, BI Technologies and ISOCOM components. We offer a wide variety of fiber optics, laser diodes and modules. Plus find thousands of photocouplers for every application, including IGBT and MOSFET gate driver, triac and SCR output, and transistor and phtotovoltaic output photocouplers. We also carry a large selection of photoelement components such as photointerrupters, diodes and transistors. Optoelectronic devices convert back and forth between electrical and optical signals. Due to the prevalence of CMOS devices, both analog and digital signals are most easily processed and stored in electronic form. However, optical signals provide distinct advantages for high-speed and long-distance transmission. The two key technologies for converting electrical signals to optical are light-emitting diodes (LEDs) and lasers. LEDs use current flowing through a PN junction to emit photons. This junction can be engineered to produce any desired spectrum of light. Lasers also convert electricity into visible light, but can produce a coherent, more spectrally pure, and more powerful light source. Lasers require more electrical power than LEDs. A laser diode is a device that has qualities of both a laser and an LED. Converting optical signals into electrical signals is accomplished via a photodiode or photovoltaic cell. Many optoelectronic systems mimic their purely electronic counterparts. There are optoelectronic switches, transceivers, and multiplexers. They perform the same basic functions but have either optical inputs, outputs, or both. These optoelectronic systems are comprised of LEDs, lasers, laser diodes, and photodetectors.
21,142
총 제품