개발 시스템

Shop Arrow.com for electronics development systems from top manufacturers including Arduino, Infineon, Microchip, NVIDIA, NXP, STMicroelectronics, Qualcomm and Raspberry Pi. We are an authorized distributor of new and popular programmers, emulators and debuggers, software development tools, and evaluation boards for a wide range of applications and projects. Development systems are tools used by design engineers to implement software or hardware. Systems with a microprocessor (MPU) or microcontroller (MCU) present will require their use. In any development system, there is the concept of a “target”. A target is what software or hardware (in the case of programmable logic) will run on. This target can be the actual hardware and software environment that the design will operate inside, or it can be a hardware and or software machine that emulates it. In the case of using the actual end target in a design, many systems have special interfaces built in to enable access. These include physical interfaces like JTAG which allow access to the subsystems and I/O of the microprocessor with a technique called boundary scan. Physical debug modules can also be built into an MPU or MCU to allow for the internal registers to be read and updated, the program counter to be stepped, and address and data buses to be accessed. Memory is usually accessible and subsystems like the internal cache may have additional circuitry to assist in profiling code during run-time. If the actual hardware is not available, chip manufacturers and third party design houses produce development kits. These are generic platforms that enable designers to prototype on a platform that has similarities to the ultimate target. There are hardware platforms available for most targets, including microprocessors and programmable logic devices. Designers developing MPUs have the opportunity to simulate the device on logic simulators, which are programs that interpret the hardware description language, run the design through a set of test stimulus and output the results. In some cases teams can download the hardware design to a programmable logic platform to test, usually at a slower clock rate than the ultimate design. Software development systems incorporate simulators to emulate the target, but can also include an in-circuit emulator (ICE) physical connections for debugging. Designers writing in a high level language (like C) have debugging environments that can display the underlying assembler language and watch the state of variables and memory. Virtual machines can be used to decouple the computer the designer is using from the design and target the correct operating system. Designers also write algorithms, and these can be tested in mathematical modeling programs like Matlab. Mathematical models can extend to emulate whole systems (for example, Simulink). Circuit designers have the option of testing analog circuits in packages like SPICE and physical electromagnetic simulation. These tools can be connected to real-life measurement systems to obtain performance characteristics and improve modeling.

1,092

총 제품

모두 보기