Decoders and Demuxes
A demultiplexer is a type of electrical routing device and is used it both analog and digital circuitry. For inputs, it has a single signal line and for outputs it has two or more signal lines. Its purpose is to route a single input signal into a particular output channel. The channel is determined by selector inputs, which represent a unique output channel.
Demuxers are often used in conjunction with multiplexers to provide a routing methodology, which saves space in a layout when there are a high amount of data channels. A mux selects from multiple inputs and route that to a single output. That output then goes to the input of the demux and be sent to a specific, selected output. In many cases, this saves a considerable amount of space.
A decoder is a device, which activates an output channel unique to a particular logical value applied to the selection lines. Demuxers can also be used as a decoder device for digital inputs. If the signal of entry is always a logical 1, then the selection lines can be used to route that value through to the appropriate output line. This type of decoder device is called a 1 to n device. Only one output channel at any specific time is routed to the input.
1,804
Total Products