Resistor Networks and Arrays
A simple resistor network is one in which a group of resistors is laid out in series (end to end) and a power source is connected to one side whereas the other is grounded. Each conductive node between each resistive element will have a lower voltage value than the previous (starting from a positive voltage source). This allows precise voltage levels to be tapped and utilized instead of complex DC-to-DC conversion being required. Inherent resistor capabilities also allow for far more complex networks to be designed. Often an electric device called a DAC (digital to analog converter) use a network called a resistor ladder to take in digital inputs and read out certain nodes to create an analog signal out.
Resistor networks and arrays contain two or more resistive elements arranged in a variety of patterns. There are many potential uses for a specific pattern of resistors because of their inherent ability to change the voltage and current within a system. The power and importance of these networks comes through tapping to different nodes within the network. The nodes in a resistive array that aren’t at ground or main power will have voltage and current characteristics which are unique and that result from the specific arrangement and values of each resistor.
332,522
Total Products